============================================================
                            Universal Library
                    Measurement Computing Corporation
     ============================================================


1. Introduction
2. Windows
3. Android
4. Known issue
5. Support policy and how to contact us


==========================================
1. Introduction
==========================================
The Universal Library provides a fast, simple, and powerful API that allows
programmers and engineers to develop sophisticated data acquisition applications 
using various programming languages. 


==========================================
2. Windows
==========================================
InstaCal is an easy to use installation, calibration and test software that 
minimizes the time between set up and actually making measurements.

Requirements
  Microsoft Windows 10/8/7/Vista/XP operating system (32-bit/64-bit versions)*
   (Windows 7 requires SP1 and the latest Windows updates; XP requires SP3) 
  Microsoft .NET Framework 2.0 or later (required only for the UL .NET class libraries)
  Intel Pentium III class processor, 500 MHz or higher
  Video display  800 x 600, 256 colors or greater
  Minimum of 256 MB of RAM (512 MB or higher recommended) 
  Minimum of 125 MB of free hard disk space 
  Microsoft-compatible mouse
  Windows Installer version 1.1 or later 


* For 64-bit Vista operating systems, see the known issue below. ISA, PC104, PPIO, 
PC-CARD (and PCMCIA) and E-PDISO16 devices are not supported on Windows 10/8/7 and 
Windows Vista.
PCI-DAS1000/1200/1600 Series devices are not supported for 64-bit operating systems.


==========================================
3. Android
==========================================
Android sample programs may be installed on Windows platforms for deployment to 
Android platforms using a design environment such as Eclipse.

Compiled versions of some of these samples can be downloaded directly to your 
Android device from the Google Play Store.

Requirements

  Android 3.1 platform (API level 12) and later. 

If deploying from Windows, see Windows requirements above.


==========================================
4. Known issue
==========================================
Due to a driver compatibility issue, using the Universal Library on Windows Vista 64-bit
operating system requires one of the following:

1. Universal Library version 6.55 or earlier, or 
2. Disable driver signing verification in Windows Vista 64 (using F8 at boot or bcdedit)


==========================================
5. Support policy and how to contact us 
==========================================
Please contact Measurement Computing for information on technical support.

Measurement Computing
10 Commerce Way
Norton, MA 02766
Phone: (508) 946-5100
Fax: (508) 946-9500
www.mccdaq.com

You may check for the latest version of the Universal Library from our download site 
at http://www.mccdaq.com/software.aspx. 

Universal Library is a trademark of Measurement Computing Corporation.
Windows is a registered trademark of Microsoft Corporation.